Specify a Local System ID (Outstation Set)

Use the Local System ID fields on the Kingfisher tab to enable and enter a Local System ID. This ID replaces the Kingfisher network System ID that you set in the Kingfisher Server Configuration (see Specify the System ID). The Local System ID is used to synchronize messages between the outstation and Geo SCADA Expert.

Use Local System ID

Select this check box to enable the Local System ID. Clear the check box to disable the Local System ID.

Local System ID

The ID character. Enter as a hexadecimal number. For example, 2A.

Further Information

Specify a Local System ID (Outstation).


Disclaimer

Geo SCADA Expert 2022