Blink
Associated with: Tables, including CDBHistoric and CDBHistoricAll (but not Data Grid tables, the Event Journal (CDBEventJournal), or other Historic Pseudo tables); optional for Data Tables
Some system colors
If the Foreground field is included without the Blink field, none of the List’s entries will flash when a flashing system
The Blink field has no effect if it is included in the SELECT Clause without the Foreground field.
(To ascertain whether Blink is used in a particular Data Table, look at the Attributes of the fields in that table (see Specify the Field Properties in the Geo SCADA Expert Guide to Core Configuration.)
If required, you can assign a Blink alias to one or more fields, in order for only the entries in certain columns to flash (see Lists in Which only the Entries in Particular Columns Change Color).