Display a List
There are various ways of displaying a List.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
You can also:
- Display a Client-Wide Alarms List (for information on Alarm Lists, see the Geo SCADA Expert Guide to Alarms)
- Display a General List of Events
- Display a Queries List from the Queries Bar
- Display the Data on a Data Grid, Data Set, or Data Table in List Format
- View and Action Lists on an Original WebX client.
Many Lists display instantaneously. For those Lists for which a large number of records need to be retrieved, Geo SCADA Expert provides a progress report while that data retrieval is ongoing. This report is updated in real time and indicates the number of records that have been retrieved so far. The report is replaced by the List entries as soon as the relevant records have been retrieved. You can continue to perform other activities in Geo SCADA Expert while such data retrieval is ongoing. To cancel a request to display a List containing a large number of records, close the progress report window.
We strongly recommend that the Guest user account is not used for operator access. As part of this restriction, access to Queries Lists might be prohibited for the Guest User on your system. This is indicated by a diagnostic message being displayed if a user attempts to display a List such as an Events List, Historic List, or Queries List without logging on. To access such a List on a ViewX client on such a system, you have to log on using a valid User Account that has the relevant permissions and access. For more information, see Specify Whether the Guest User can Execute SQL Queries.