Filter Condition Types

When you display a List such as an Alarm Summary, Events List, Queries List, or Historic List, you can filter the List so that it only shows entries that match specified criteria (see Add a Filter to a List). This is useful as it allows you to control what information is shown on a List so that the data is relevant to your current requirements.

When you are configuring a filter for a List, you need to choose a type of filter condition. The filter condition restricts the entries that are included in the List—the List only shows those items, alarms, or Events that match the defined criteria.

The filter conditions that are available for selection vary according to the type of database field (string, time, numeric, and so on) to which you are applying the filter. Depending on the type of field, you can choose from the following filter conditions:


Disclaimer

Geo SCADA Expert 2022