Add Variables to a Ladder Diagram
Each value that is read or written by your Ladder Diagram is represented by a variable or a constant. Constant values are fixed values and are described in Add a Constant Value to a Ladder Diagram. Variable values change according to the data that is stored in your system and the calculations that are performed on it.
There are 2 types of variable:
- Internal variables are values that are used by the program but are not written to an item in the database. For example, values that are used in a conversion.
- Direct variables are values that are stored in the database, for example, a point value.
For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.