Add a Transition to a Sequential Function Chart

Transitions represent a condition such as an item being in a specific state, or a value being in a specific range. The step that follows the transition is only activated if the condition defined in the transition is true.

For more information, see Transitions.

To add a transition to a Sequential Function Chart:

  1. Display the SFC in Design mode (see Display a Sequential Function Chart).
  2. Right-click on the background of the SFC.
    A context sensitive menu is displayed.
  3. Select the Add Transition option.
    The transition is added to the SFC

You can edit the transition by right-clicking on it and selecting the Edit option from the context sensitive menu (see Edit a Transition).


Disclaimer

Geo SCADA Expert 2022