COS
Function Name |
COS |
---|---|
Description |
Converts a REAL or LREAL input into a cosine value that is the output. The cosine value is also a REAL or LREAL. |
Arguments |
Input 1 {REAL or LREAL}. This value is in radians. For more information on the data types for the inputs and outputs, see Data Type Hierarchy. |
Returns |
Output {REAL or LREAL} |
Example:
Function Block Diagram - COS:
In this example, the input of 5 is provided by the CurrentValue
property of a point. The COS function converts the value into a cosine value of 0.283662185463226 and this is used as the output.
ST Program - COS:
The syntax for a COS function in an ST Program is:
Output := COS (Input 1);
Where Output and Input 1 are defined as variables earlier in the ST program. The Input 1 variable represents a REAL or LREAL type of value (the output is the same type of value as Input 1).