Coding and Test

Logic programs must be written by persons who have the necessary skills and knowledge related to the understanding, construction and operation of such programs. This knowledge includes, but is not limited to, having a thorough understanding of:

Badly designed Logic programs can cause:

Before using a Logic program in a 'live' system, thoroughly test all aspects of that program using a test system that accurately reflects the real system (including database size and data retrieval frequency). Perform further tests once the Logic program is installed on the real system to verify the correct operation of that program. It is important that arrangements for such checks are made and that sufficient time is allowed to perform complete and satisfactory testing.

WARNING

UNEXPECTED BEHAVIOR OF APPLICATION

Thoroughly test and monitor Logic programs:

  • In a simulated environment that accurately reflects the real system
  • In the real environment

before relying on the operation of those programs in a 'live' system.

Failure to follow these instructions can result in death, serious injury, or equipment damage.

Store all documentation for future reference.


Disclaimer

Geo SCADA Expert 2022