Default Values for Built-in Data Types (Literals)

The format for entering default values for integer, real, bit, string, time, and date and time variables is:

VAR

<Value name> : <data type> := <default value>;

END_VAR

Example:

The following example shows how default values can be set for a variety of built-in data types:

VAR

a: INT:= 535;

d: DATE:= D#2004-06-21;

t: TIME_OF_DAY:= TOD#12:30:07;

n: TIME:= T#1h30m;

p: ARRAY[1..4] OF INT:= [10,90,12,14];

q: ARRAY[1..100] OF REAL:= [100(20.5)];

END_VAR;

The default value for the q variable sets 100 array values to have a default value of 20.5.


Disclaimer

Geo SCADA Expert 2022