Delete a Variable on a Ladder Diagram

You can use the Delete option to remove unwanted variables from your Ladder Diagram.

To delete a variable on a Ladder Diagram:

  1. In the Variables list above the Ladder Diagram, right-click on the variable you want to delete (on the Direct tab or Internal tab as appropriate).
    A context sensitive menu is displayed.

  2. Select the Delete option.
    If the variable is referenced, a confirmation window is displayed.

  3. Either:
    • Select Yes to confirm the deletion and close the confirmation window.
      The variable is removed from the diagram.

    Or:

    • Select No to cancel the deletion.

Disclaimer

Geo SCADA Expert 2022