Disable Execution

Associated with: ST Programs, Function Block Diagrams, Ladder Diagrams, Sequential Function Charts

Security permission required to access this pick action: Configure

The Disable Execution action allows you to set a Logic program so that it cannot be executed. Once you have selected the Disable Execution action for a Logic program, the program’s Execute method cannot be triggered (and the Execute action cannot be selected).

If you use the Disable Execution action on a Logic program, that program will be unable to execute again until its Enable Execution action is selected. If you select the Enable Execution action, the Execute action and method for the Logic program become available again, and so the Logic program can be triggered to execute when required.

You can see whether a Logic program has had its execution status set to disabled by using the Status Display (the Execution status shows Enabled or Disabled). For more information, see Logic Specific Status Attributes.


Disclaimer

Geo SCADA Expert 2022