EXTRACT_DT_YEAR

Function Name

EXTRACT_DT_YEAR

Description

Converts a Date and Time input into an integer output for the year.

Arguments

Input 1 {DATE_AND_TIME}

Returns

Output {INT}

The output is the year part of the Date and Time input.

Example:

Function Block Diagram - EXTRACT_DT_YEAR:

An EXTRACT_DT_YEAR function has an input of NOW. This sets the input to be the current date and time. The EXTRACT_DT_YEAR function returns the year part of the date in the Date and Time input as its output. So, if the date and time value of the input was 2006-03-21-10:25:00.000, the EXTRACT_DT_YEAR function would return 2006 (the year part of the Date and Time input).

ST Program - EXTRACT_DT_YEAR:

The syntax for an EXTRACT_DT_YEAR function in an ST Program is:

Output := EXTRACT_DT_YEAR (Input 1)

Where Output is an integer value and Input 1 is a Date and Time value.


Disclaimer

Geo SCADA Expert 2022