MIN

Function Name

MIN

Description

Outputs the same value as its lowest input.

Arguments

Input 1 - Input n {ANY}

For more information on the data types for the inputs and outputs, see Data Type Hierarchy.

Returns

Output {ANY}.

The MIN function outputs the same value as its lowest input. The output is of the same type as the input.

Example:

Function Block Diagram - MIN:

In this example, the inputs are constant values. The MIN function outputs the same value as its lowest input. In this case, it has inputs of 4 and 5, so it outputs 5.

ST Program - MIN:

The syntax for a MIN function in an ST Program is:

Output := MIN (Input 1, Input n);

Where Output, Input 1 and Input n are defined as variables earlier in the ST program.


Disclaimer

Geo SCADA Expert 2022