Disable Device
Associated with: MQTT JSON Schema A Device items
Security permission required to access this pick action: Disable Points
Use this pick action to take an MQTT JSON Schema A Device item Out of Service.
The Disable Device pick action clears the Device's In Service property, so that the Device is no longer active.
You might want to disable a Device database item, for example, if Geo SCADA Expert has detected a problem with the publishing device that the database item represents. Once the problem has been rectified, use the Enable Device pick action to place the Device back In Service.
Geo SCADA Expert logs an entry in the Event Journal whenever either pick action is used. The entry indicates whether the Device has been enabled or disabled.
Be aware that disabling an MQTT JSON Schema A Device also de-activates its dependants, although their configuration will remain unchanged. Dependants include items such as points that are associated with the Device.
When the Device is disabled, Geo SCADA Expert unsubscribes from the topic, and so no longer receives messages relating to that topic.
If using this pick action with the Automation Interface, you need to specify the method name Disable.