Minimum Configuration

This topic relates to points on the MQTT JSON Schema A driver.

When you add an item to the database, various properties on the item's configuration Form are assigned a value automatically. These default values are assigned on creation of the database item, to help reduce the amount of manual configuration that is required. As such, you only need configure a subset of the properties that exist on an item's configuration Form. Typically, the properties you have to configure include:

 

For a point on this driver to be capable of functioning in Geo SCADA Expert, as a minimum you have to specify these properties on the point's configuration Form (the properties are on the <Point Type> tab unless stated otherwise):

 

If you want to store the point data historically, you have to:

 

Also ensure that the the database items on which the point depends are In Service, and have saved, valid configuration. This will produce a point that is capable of functioning using the default configuration settings.


Disclaimer

Geo SCADA Expert 2022