Actions that are Specific to the MQTT Sparkplug™ B Driver

This driver is an extension driver. As such, it supports a combination of the pick actions that are supported by its 'parent' driver, in addition to its own driver-specific pick actions. Use this section in conjunction with the 'parent' driver documentation for comprehensive information about the pick actions that are supported by this extension driver.

The topics in this section explain those pick actions that are specific to the MQTT Sparkplug B driver. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Before performing any controls, ensure that you familiarize yourself with the additional checks that you should perform when executing controls on the MQTT Sparkplug B driver (see Actions that are Specific to MQTT Sparkplug™ B Points).

Further Information

Actions supported by this driver's parent driver: see Using MQTT Specific Actions in the Geo SCADA Expert Guide to the MQTT Driver.


Disclaimer

Geo SCADA Expert 2022