Alarm Limits
Use the fields within the Alarm Limits section of the Analog Point tab to set limits for an MQTT Sparkplug™ B analog point and specify whether an alarm or event is generated if the point exceeds those limits.
For information on configuring Alarm Limits properties, including the Alarm Limits fields that are common to many analog points, see Configure the Limits for an Analog Point in the Geo SCADA Expert Guide to Core Point Configuration.
For information about the properties that appear towards the bottom of the Alarm Limits section, select the relevant links below:
-
Engineering Units Exceeded—Use to Define how Over Range and Under Range Values are Processed.
-
Tune Limits—Use to Define whether an Analog Point’s Limits can be Tuned.
-
Area of Interest—This field is only displayed if the Area of Interest feature is enabled on your system. Use the field to specify the Area of Interest with which any state-related point alarms or events are to be associated (see Specify the Area of Interest Associated with a Point’s State-Related Alarms and Events).