Configure an MQTT Sparkplug™ B EoN Node

An MQTT Sparkplug B EoN Node represents an MQTT Edge of Network (EoN) node on an MQTT Sparkplug B Broker. The node is an MQTT version 3.1.1 compliant client application that manages an MQTT session. An MQTT Sparkplug B EoN Node can be the parent of MQTT Sparkplug B Devices and/or MQTT Sparkplug B Points.

You configure the properties of each MQTT EoN Node using the fields on the MQTT Sparkplug B EoN Node configuration Form. The Form has several tabs, some of which contain properties that are common to many database items, and others that contain properties that are specific to MQTT Sparkplug B EoN Nodes.

The topics in this section document the properties that are on the EoN Node tab (see Configure the Properties on the EoN Node Tab).

The properties on the remaining tabs are common to many database items. For information about those tabs, see Tabs that are Common to Many Configuration Forms.


Disclaimer

Geo SCADA Expert 2022