Enable EoN Node

Associated with: MQTT Sparkplug™ B EoN Nodes

Security permission required to access this pick action: Disable Points

Use this pick action to place an MQTT Sparkplug B EoN Node In Service. Triggering the action changes the EoN Node's configuration so that its In Service property is enabled and the EoN Node becomes active.

When the EoN Node is enabled, Geo SCADA Expert processes any messages that it receives from that node. This occurs providing that the Broker, Group, and EoN Node database items are In Service and have valid, saved, configuration, and Geo SCADA Expert is able to connect successfully to the broker.

The Enable EoN Node pick action is only available for an MQTT Sparkplug B EoN Node:

Also see Disable EoN Node.

If using this pick action with the Automation Interface, you need to specify the method name Enable.


Disclaimer

Geo SCADA Expert 2022