Errors When Create Points Last Ran
Associated with: MQTT Sparkplug™ B EoN Nodes and MQTT Sparkplug B Devices
This status attribute indicates whether Geo SCADA Expert detected any issues when the Create Points from Birth Metrics pick action was last executed on the selected EoN Node or Sparkplug B Device.
A value of 0 (zero) indicates that the point creation process that was last triggered by the Create Points from Birth Metrics pick action completed successfully.
If a value other than 0 is displayed, look at the entries in the Alarms List and Events List to ascertain the issues that occurred. The entries will be assigned the Sparkplug B Configuration Error category (see Alarm and Event Categories that are Specific to the MQTT Sparkplug™ B Driver).