Online State

Associated with: MQTT Sparkplug™ B EoN Nodes and MQTT Sparkplug B Devices

Use this Online State status attribute in conjunction with the Online State Alarm attribute to ascertain the connection status of the selected MQTT Sparkplug B EoN Node or Device.

With an MQTT Sparkplug B EoN Node, the possible values of the Online State status attribute are:

With an MQTT Sparkplug B Device, the possible values of the Online State status attribute are:

Also see Online State Alarm.


Disclaimer

Geo SCADA Expert 2022