Status Attributes that are Specific to the MQTT Sparkplug™ B Driver

This driver is an extension driver. As such, it supports a combination of the status attributes that are supported by its 'parent' driver, in addition to its own driver-specific status attributes. Use this section in conjunction with the 'parent' driver documentation for comprehensive information about the status attributes that are supported by this extension driver.

The topics in this section explain the status attributes that are specific to items on the MQTT Sparkplug B driver. For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.

Further Information

Status attributes supported by this driver's parent driver: see Status Display Attributes that are Specific to the MQTT Driver in the Geo SCADA Expert Guide to the MQTT Driver.


Disclaimer

Geo SCADA Expert 2022