Define the Script Settings for a Mimic

You can use the Mimic Properties window to enable client-side scripting for a Mimic and also to access the Script Editor which you can use to create a Mimic script. The Mimic Properties script settings are:

The Script settings are only available when you display the Mimic Properties window for an individual Mimic (rather than via the Options window).

For more information, please see Mimic Scripts in the Geo SCADA Expert Guide to Scripting.


Disclaimer

Geo SCADA Expert 2022