Editing a Pipe
            When you have added a pipe object to a Mimic, you can access its Pipe Properties window to edit its settings. To display the window, double-click on the object on the Mimic. (For other ways of displaying the window, see Display the Properties Window for an Object on a Mimic.)
                
            
The Pipe Properties window contains two tabs:
- General—The General tab contains some common settings for General tabs, including Name, Visible, Animations, Pick Action, ToolTip, and the Dynamic Position settings. For more information on these settings, see General Tab.
 - Fill—Use the Fill tab to define the color and shading settings for the background of the pipe. The Fill tab settings work in the same way as the settings on other Fill tabs (see Fill Tab).