Embedded Mimic Animations
Each embedded Mimic has the following properties that you can animate as required:
- MaintainAspectRatio—see MaintainAspectRatio.
- PickComment—see PickComment Animations.
- PickDisabled—see PickDisabled Animations.
- PickParam—see Pick Action Animations for Mimic Objects if you are configuring an embedded Mimic on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring an embedded Mimic on a Symbol Mimic.
- PickType—see Pick Action Animations for Mimic Objects if you are configuring an embedded Mimic on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring an embedded Mimic on a Symbol Mimic.
- PosAnchor—see Position Animations.
- PosMax—see Position Animations.
- PosMin—see Position Animations.
- PosVal—see Position Animations.
- Shared—The shared animation property corresponds to the Shared with other embedded Mimics setting on the Embedded Mimic Properties window. Although it is possible to animate the Shared property (it can be True or False), it is not designed for use as an animation.
- TooltipText—see ToolTipText Animations.
- Visible—see Visibility Animations.