Embedded Query List Animations
You can animate the properties of an embedded List on a Mimic. Although embedded Lists have unique properties, some of the properties are similar to those of other objects and can be used for similar types of animation.
You can animate the following properties for an embedded List:
- BackColour—see BackColour.
- Font—see Font Animations.
- GridColour—see GridColour.
- GridSize—see GridSize.
- HeaderDkShadowColour—see HeaderDkShadowColour.
- HeaderFaceColour—see HeaderFaceColour.
- HeaderFont—see HeaderFont.
- HeaderHighlightColour—see HeaderHighlightColour.
- HeaderShadowColour—see HeaderShadowColour.
- HeaderTextColour—see HeaderTextColour.
- PickComment—see PickComment Animations.
- PickDisabled—see PickDisabled Animations.
- PickParam—see Pick Action Animations for Mimic Objects if you are configuring an embedded List on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring an embedded List on a Symbol Mimic.
- PickType—see Pick Action Animations for Mimic Objects if you are configuring an embedded List on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring an embedded List on a Symbol Mimic.
- PosAnchor—see Position Animations.
- PosMax—see Position Animations.
- PosMin—see Position Animations.
- PosVal—see Position Animations.
- Sql—see Sql.
- System—see System.
- TextColour—see TextColour.
- TooltipText—see ToolTipText Animations.
- Visible—see Visibility Animations.