Embedded Trend Animations
You can animate the properties of an embedded Trend on a Mimic. Although Embedded Trends have unique properties, many of their properties are similar to those of other objects and can be used for similar types of animation:
- BackAlpha—see BackAlpha.
- BackColour—see BackColour.
- LabelFont—Represents the text properties of the embedded Trend's label. These properties work in the same way as Font Animations.
- MainFont—Represents the text properties of the values shown on the axes of the embedded Trend. These properties work in the same way as Font Animations.
- PickComment—see PickComment Animations.
- PickDisabled—see PickDisabled Animations.
- PickParam—see Pick Action Animations for Mimic Objects if you are configuring an embedded Trend on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring an embedded Trend on a Symbol Mimic.
- PickType—see Pick Action Animations for Mimic Objects if you are configuring an embedded Trend on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring an embedded Trend on a Symbol Mimic.
- PosAnchor—see Position Animations.
- PosMax—see Position Animations.
- PosMin—see Position Animations.
- PosVal—see Position Animations.
- TitleFont—Represents the text properties of the title text. These properties work in the same way as Font Animations.
- TooltipText—see ToolTipText Animations.
- Visible—see Visibility Animations
- XAxisVisible—see Visibility Animations
- YAxesVisible—see Visibility Animations.