Embedded X-Y Plot Animations
You can animate the properties of an embedded X-Y Plot on a Mimic. Although Embedded X-Y Plots have unique properties, many of the properties are similar to those of other objects and can be used for similar types of animation.
You can animate the following properties for an embedded X-Y Plot:
- BackAlpha—see BackAlpha.
- BackColour—see BackColour.
- LabelFont—Represents the text properties of the embedded X-Y Plot's label. These properties work in the same way as Font Animations.
- MainFont—Represents the text properties of the values shown on the axes of the embedded X-Y Plot. These properties work in the same way as Font Animations.
- PickComment—see PickComment Animations.
- PickDisabled—see PickDisabled Animations.
- PickParam—see Pick Action Animations for Mimic Objects if you are configuring an embedded X-Y Plot on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring an embedded X-Y Plot on a Symbol Mimic.
- PickType—see Pick Action Animations for Mimic Objects if you are configuring an embedded X-Y Plot on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring an embedded X-Y Plot on a Symbol Mimic.
- PosAnchor—see Position Animations.
- PosMax—see Position Animations.
- PosMin—see Position Animations.
- PosVal—see Position Animations.
- TitleFont—Represents the text properties of the title text. These properties work in the same way as Font Animations.
- TooltipText—see ToolTipText Animations.
- Visible—see Visibility Animations.