Enable or Disable Anti-Aliasing for a Specific Mimic

You can use the Mimic Properties window to enable or disable the Anti-Aliasing feature on an individual Mimic. To do this, you use the Mimic Properties window that you access via the Properties option or command on the Mimic. The setting that you put in place will only apply to the Mimic you are configuring and will apply every time the Mimic is displayed. However, if you enable the Anti-Aliasing feature for a Mimic, it will only be used if that Mimic is displayed on a client PC that is configured to use Anti-Aliasing (see Enable or Disable Anti-Aliasing for your Client PC). If the client PC is not configured to use Anti-Aliasing, the Anti-Aliasing feature will not be applied irrespective of the Mimic’s configuration settings.

To enable or disable Anti-Aliasing for an individual Mimic:

  1. Display the Mimic in Design Mode (see Displaying a Mimic).
  2. Display the Mimic Properties window for that particular Mimic (see Defining the Default Mimic Properties for a Specific Mimic).
    The settings on the Mimic Properties window only apply to the Mimic that you are currently configuring.
  3. On the Mimic tab of the Mimic Properties window, use the Anti-Alias check box to define whether Anti-Aliasing is enabled or disabled on the Mimic:
    • Select the check box to enable the Anti-Aliasing feature for the Mimic
    • Clear the check box to disable the Anti-Aliasing feature for the Mimic.
  4. Close the Mimic Properties window.

If you access the Mimic Properties window via the Options window, the changes you make will apply to new Mimics on your client PC, not just the Mimic you have on display.


Disclaimer

Geo SCADA Expert 2022