Moving the Mimic within the Display (Panning)
You can use the Pan tool to move a Mimic within the ViewX Document Display Area or Virtual ViewX Document Display Area. This is useful when you want to look at another part of a Mimic without changing the level of magnification.
To pan a Mimic:
- Activate the Pan tool:
In ViewX or Virtual ViewX, select Pan Mode in the Navigation command group on the Home tab.

You can also right-click on the background of the Mimic to display a context-sensitive menu, then select the Pan option.
- Select any area on the Mimic and keep the left-hand mouse button pressed down.
- Move the cursor to move the Mimic within the ViewX Document Display Area.
- Release the left-hand mouse button when the required part of the Mimic is shown.