Pipe Animations
You can animate the following properties for pipe objects:
- Fill—see Fill Animations.
- PickComment—see PickComment Animations.
- PickDisabled—see PickDisabled Animations.
- PickParam—see Pick Action Animations for Mimic Objects if you are configuring a shape on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring a shape on a Symbol Mimic.
- PickType—see Pick Action Animations for Mimic Objects if you are configuring a shape on a 'normal' Mimic, and see Pick Action Animations for Symbols if you are configuring a shape on a Symbol Mimic.
- PosAnchor—see Position Animations.
- PosMax—see Position Animations.
- PosMin—see Position Animations.
- PosVal—see Position Animations.
- TooltipText—see ToolTipText Animations.
- Visible—see Visibility Animations.
- Width—see Width.