Removing or Disabling a Pick Action Association
            You can use the Pick Action Wizard to delete a pick action association so that a Mimic object no longer provides access to pick action functionality. For example, if a Mimic object provides access to an Object Menu, you can remove or disable the pick action configuration so that selecting the Mimic object has no effect.
When canceling a pick action association, you have 2 options:
- You can remove the pick action association completely, so that the configuration for the pick action is removed and the Mimic object is not associated with the pick action in any way.
 - You can disable the pick action association so that the pick action configuration remains intact, but is disabled. This means that the Mimic object will not 'trigger' the pick action when selected. However, if the pick action is disabled, it can later be restored by clearing the Disabled check box—the pick action will not need to be reconfigured.
 
To remove or disable a pick action association:
- Display the Pick Action Wizard for the Mimic object that you wish to disassociate from the pick action (see Accessing the Pick Action Configuration Wizard).
 - On the first 'page' of the Wizard, either:
            
- Select the None option to remove the pick action configuration. You should select this option if you want to cancel the pick action association permanently.
 
Or:
- Select the Disabled check box to leave the pick action configuration in place, but set it to be disabled so that selecting the Mimic object has no effect. You should use this option if you only need to temporarily cancel the pick action association.
 
 - Select the Next button to proceed to the next 'page' of the Pick Action Wizard.
 - Repeat step 3 as required until you reach the final 'page' of the Pick Action Wizard.
 - Select the Finish button to confirm your selections and close the Pick Action Wizard.