Set the Size and Orientation of a Mimic

You can use the Mimic Properties window to change the size and orientation of a Mimic so that it has different dimensions. For example, you can set a Mimic to be the same size as A5 paper and to have landscape orientation. This is useful when you need to print out Mimics on different paper sizes.

Depending on the method that you use to display the Mimic Properties window, the settings you define will be applied to:

When you have displayed the Mimic Properties window using the appropriate method for your needs, define the size settings as follows:


Disclaimer

Geo SCADA Expert 2022