Using the Animations Window to Set Up Pick Actions
            You can use the Animations window to set up pick actions. This is useful when you need the availability of a pick action to be dependant on a condition. For example, you can use an animation expression to set a pick action menu to only be available when a point is in a specific state.
There are several animation properties that relate to pick actions, including:
- PickComment—Use to animate the comment for a pick action.
 - PickDisabled—Use to enable and disable a pick action with an animation.
 - PickParam—Use to animate the features of the pick action menu.
 - PickType—Use to set the type of pick action menu (Geo SCADA Expert Object, Hyperlink, Registry, and so on).
 
For more information on setting up the pick action animations, see Animations.