Configuration Examples

This section includes examples of Geo SCADA Expert configuration that might be used to allow the Geo SCADA Expert Mitsubishi driver to transmit data to and from Mitsubishi MELSEC A PLCs.

The examples refer to specific address ranges within each PLC—for more information on the type of data and the corresponding address ranges within each type of PLC, see Mitsubishi Data Address Ranges.

The address range with which a channel, scanner or point is associated is displayed as part of the Source status attribute. The Source attribute is displayed on the associated List and Status display for each item (see Mitsubishi Specific Status Display Attributes).

Use the examples as an aid when configuring your Geo SCADA Expert system. The examples in this section include:


Disclaimer

Geo SCADA Expert 2022