Configure the Primary and Secondary Port Properties

Use the fields on the Primary Port and Secondary Port tabs to specify how many ports are available to a scanner, the port number, communications protocol, and the address of the Modbus device that is to be scanned.

For an example of scanner configuration that uses Network communications and the Modbus RTU protocol, see Use Modbus RTU to Communicate via a Terminal Server.


Disclaimer

Geo SCADA Expert 2022