Test Your Knowledge on the WebX Interface

ATTENTION: This topic relates to the deprecated Original WebX client that is supported by this and previous versions of Geo SCADA Expert. For information about the Virtual ViewX client that is supported by Geo SCADA Expert 2019 onwards, for which the web server is hosted using IIS, click here.

How much do you know about the WebX interface? Try and answer the following questions:

  1. WebX is designed to allow remote access, but can it be used to access your system from anywhere?
  2. Apart from remote access and appearance, what is the main difference between WebX and ViewX?
  3. What features are used to help prevent unauthorized access via a WebX client?
  4. How do you access WebX?
  5. If you don’t have a mouse with a wheel, how can you zoom in on a Mimic in WebX?
  6. You can use your web browser’s Back and Forward buttons to navigate through WebX displays in the order in which you originally displayed them. But what other ways are there of accessing different WebX displays?
  7. You want to display status information about a specific point. How would you do this in WebX?
  8. You are logged on via a WebX client when an alarm is raised. You are responsible for responding to the alarm, so what do you do?
  9. How can you filter the Alarms List so that it only displays alarms that relate to items in a specific Group?
  10. You display the Events List and its entries are sorted in Time order. You want them to be sorted according to their Severity and so create a new Severity sort method. You apply the Severity method but the Events List still appears to be sorted according to time. Do you know why?
  11. You want to perform a Hand Control on a database point via WebX. How would you achieve this?

Disclaimer

Geo SCADA Expert 2022