Add your SQL Query to QueryPad

To test an SQL query in QueryPad, you need to add your query to the SQL Entry Pane.

The SQL Entry Pane is in the lower part of the window

There are two ways of doing this, either:

Or:

When you have added your SQL Query to QueryPad, you can proceed to test it (see Run your Query in QueryPad).


Disclaimer

Geo SCADA Expert 2022