Working with QueryPad
QueryPad is an SQL query diagnostics tool that runs independently of ViewX and is supplied as part of your Geo SCADA Expert software solution. It allows you to test your SQL queries and provides details that may help you to improve the efficiency of your queries (and therefore improve performance). For more information, see the topics that are listed in the gray footer section at the bottom of this topic. Select the relevant entry to display the topic that you require.
Access to QueryPad might be restricted on your system. In order to connect QueryPad to a database successfully, the Geo SCADA Expert server has to be configured to allow SQL queries to be edited from its clients, and your User Account has to be configured to allow you to edit SQL queries. For more information, see Specify Whether SQL Queries can be Edited using the Clients on this Server, and see Define the SQL Editing Settings for a User.