Introduction to the ROC Plus Driver

This driver is a simple driver. It provides additional functionality to enable Geo SCADA Expert to interface with specific supported devices using a particular protocol. To interact successfully with such devices, you need to:

Intended Audience

This guide is intended for engineers that are tasked with configuring Geo SCADA Expert to communicate with supported Emerson Remote Operations Controller (ROC) devices using the ROC Plus Protocol.

The guide assumes an advanced level of expertise with Geo SCADA Expert, Microsoft Windows, electronic flow measurement, and Emerson Remote Operations Controller (ROC) devices.

Document Scope

This guide explains how to install and configure database objects on the Geo SCADA Expert ROC Plus Driver.

Geo SCADA Expert is a flexible and extensible SCADA host platform that can be used for a multitude of purposes, including gathering data from and controlling remote devices. The Geo SCADA Expert ROC Plus Driver extends the core functionality of Geo SCADA Expert to enable it to communicate with Emerson Remote Operations Controller (ROC) devices, using the ROC Plus Protocol. The driver enables Geo SCADA Expert to communicate with supported Emerson ROC devices, including ROC809 and ROC827 devices.

The Geo SCADA Expert ROC Plus driver provides a subset of the features that are available using Emerson’s custom ROC Plus Protocol, with a bias towards gathering historical data from ROC flow computers.

With the Geo SCADA Expert ROC Plus driver, you can:

ATTENTION: The level of technical information in this guide is for users who have an advanced level of expertise with Geo SCADA Expert, Microsoft Windows, electronic flow measurement and ROC devices.


Disclaimer

Geo SCADA Expert 2022