Check that Geo SCADA Expert Received the Test SMS Message from the Device

Perform this procedure after you Send an SMS Test Message from the SCADAPack 50 Device.

Follow this procedure to check whether Geo SCADA Expert has received the message that you sent from the SCADAPack 50 device:

  1. In the Database Bar, right-click on the SCADAPack 50 Test.Channel database item.

    A context-sensitive menu is displayed.

  2. Select the Display Events menu option.

    The Events List is displayed.

    The Events List should show the details of the SMS message that you sent from the device.

    There may be a delay between when you send an SMS message and when Geo SCADA Expert displays it in the Events List. This can be due to delays in the GSM network and the fact that the default modem poll interval in Geo SCADA Expert is 2 minutes. For more information, see SCADAPack 50 and SMS Messagingsee SCADAPack 50 and SMS Messaging

  3. Select the Close button.
  4. In the Database Bar, right-click on the SCADAPack 50 Test.Outstation database item.

    A context-sensitive menu is displayed.

  5. Select the View Status menu option.

    The Status window is displayed.

    Look at the following status attributes:

    • Source—The location of the device data source. This consists of the Outstation Name followed by the device Telephone Number.
    • DiagnosticsThere are a number of diagnostic database items. Geo SCADA Expert updates these with information contained in the SMS message.

  6. Select the Close button.
  7. In the Database Bar, right-click on the SCADAPack 50 Test Digital.Point database item.

    A context-sensitive menu is displayed.

  8. Select the View Status menu option.

    The Status window is displayed.

    Look at the following status attributes:

    • Source—The location of the point's data source. This consists of:
      • The Outstation Name
      • The device Telephone Number
      • The Point Identity.
    • Current Value—The point's current value (see Current Value in the Geo SCADA Expert Guide to Drivers).
    • Mapping to Device Point—This shows the device point to which the digital point is mapped, as well as the number of confirmed and unconfirmed configuration changes. For more information, see Device Point Mapping
  9. Select the Close button.

There may be a delay between when you send an SMS message and when the GSM network delivers it. For more information, see SCADAPack 50 and SMS Messaging.

If Geo SCADA Expert did not receive the test SMS message from the device, there are a number of diagnostic checks that you can do (see There is no Communication Between Geo SCADA Expert and a SCADAPack 50 Device).

If the Channel Event List indicates that Geo SCADA Expert received the SMS test message from the device, but did not process it, this may be because:

If you cannot resolve this anomaly, then contact Schneider Electric Support for further help.

You have now completed the tutorial.

For further information about the Geo SCADA Expert SCADAPack 50 driver, see Introducing the SCADAPack 50 Driver.


Disclaimer

Geo SCADA Expert 2022