Specify the Dial In/Dial Out Settings

You use the Dial In/Dial Out field on the PSTN tab to specify whether the Geo SCADA Expert GSM modem will be used to receive SMS messages only, send SMS messages only, or both send and receive SMS messages. Use this field if you want to reserve some modems in your system for either sending or receiving SMS messages only.

Use fields in the GSM Modems Receiving Data SMS Messages section of the SCADAPack 50 tab to define the local Geo SCADA Expert channel that the GSM network should use to deliver SMS messages to Geo SCADA Expert (see Specify the GSM Modem's Receiving Data SMS Messages Options).


Disclaimer

Geo SCADA Expert 2022