Switch Off Device
Associated with: SCADAPack 50 Outstation.
Security permission required to access this pick action: Diagnostics.
Use this pick action to put the device into Transport mode: this is a permanent Sleep state. The pick action stops the device from waking up, recording data and then sending it to Geo SCADA Expert.
To reverse the permanent Sleep state you need to physically apply a magnet to the device.
INOPERABLE DEVICE
If you are using this pick action with the Automation Interface, you need to specify the method name SwitchOffDevice.