DLOG Scan

Associated with: SCADAPack controllers on which DLOG is enabled

Security permission required to access this pick action: Retrieve Data

Use the DLOG Scan pick action to request the driver to scan a controller and retrieve its DLOG (stored SCADAPack) data records. Use this pick action to perform a DLOG scan that is in addition to the DLOG scanning that is already configured for the controller.

Unlike the automated DLOG scanning process, the action retrieves all of the DLOG data records, as the Max DLOG Requests Per Scan restriction specified for the automated process does not apply.


Disclaimer

Geo SCADA Expert 2022