Firmware Type

Associated with: SCADAPack controllers

This attribute indicates the type of firmware that is running on a controller. The attribute is displayed once a controller is or has been in communication with the server.

Example:

Telepace
(for a controller that is running Telepace firmware)


Disclaimer

Geo SCADA Expert 2022