Firmware Variant

Associated with: SCADAPack controllers

This attribute indicates the variant of the firmware that is running on a controller. The attribute is displayed once a controller is or has been in communication with the server.

Example:

DNP3 Supported
(for a controller that is running firmware that supports DNP3 functionality)


Disclaimer

Geo SCADA Expert 2022