Resume Polling

Associated with: SCADAPack controllers on which Suspend Polling is enabled

Security permission required to access this pick action: Diagnostics

The Remote Connection interface is typically used to suspend or resume polling of a SCADAPack controller. However, if Suspend Polling is enabled, you can use the Resume Polling pick action to abort any current polling suspension and resume normal polling of a controller.

The Resume Polling pick action is only available for controllers on which the ‘Suspend Polling’ feature is enabled (see Specify Whether Geo SCADA Expert can Suspend Polling of a Controller).

Use the Resume Polling pick action to force polling to resume, regardless of whether polling was suspended via the Suspend Polling pick action, or the Remote Connection interface.


Disclaimer

Geo SCADA Expert 2022