Specify the Type of Control Operation

This section applies to SCADAPack Modbus Digital Output Points only.

Use the Control Operation combo box on the Control tab to specify the type of control operation that Geo SCADA Expert is to undertake when addressing Holding Registers (see SCADAPack Point Addressing).


Choose from:


Disclaimer

Geo SCADA Expert 2022