Which Driver?

Geo SCADA Expert can communicate with SCADAPack controllers using one of several drivers. The driver that you need to use depends on the type of SCADAPack device(s) with which Geo SCADA Expert is to communicate.

With the table below, the recommended driver for each range of SCADAPack controllers is shown at the top of the section for that particular range. Some ranges of SCADAPack controllers are designed to communicate using the DNP3 protocol, whereas other ranges are designed to communicate using the Modbus protocol, or a proprietary protocol (in the case of SCADAPack 50).

With some ranges of SCADAPack controllers, Geo SCADA Expert can also communicate with those controllers using certain other drivers or protocols, however these are not the preferred option as they do not provide support for extended functionality that is specific to those controllers. Information about these alternative drivers is shown in the shaded cells, however these drivers only provide generic support for those particular ranges of SCADAPack controllers.

SCADAPack Range Intended Use Driver Protocol Further Information
386 eNET

Monitoring and control

Outstation configuration

Download of device configuration

Firmware download

Remote Firmware Download

Download of security configuration

Configuration file upload

DNP3 SCADAPack E DNP3 (using an application-specific extension)

Run the DNP3 driver along with the DNP3 SCADAPack E extension driver.

This provides more feature-specific extended functionality for 386 eNET outstations than the Modbus drivers.

Monitoring and control

Advanced Modbus Modbus

Use the 'standard' and 'Generic' Modbus database items.

(386 eNET outstations do not support the extended Modbus functionality of other ranges of SCADAPack controllers.)

Simple Modbus Modbus If both Modbus drivers provide the required functionality, consider using the Advanced Modbus driver rather than the Simple Modbus driver. This will give you more flexibility should your system requirements change in the future.
SCADAPack 50

Data retrieval

Outstation configuration

Download of device configuration

SCADAPack 50 SCADAPack 50 Run the SCADAPack 50 driver.
SCADAPack E

Monitoring and control

Controller configuration

Download of device configuration

Firmware download

Remote Firmware Download

Download of security configuration

Configuration file upload

DNP3 SCADAPack E DNP3 (using an application-specific extension)

Run the DNP3 driver along with the DNP3 SCADAPack E extension driver.

This provides more feature-specific extended functionality for SCADAPack E controllers than the Modbus drivers.

Monitoring and control

Advanced Modbus Modbus

Use the 'standard' and 'Generic' Modbus database items.

(SCADAPack E controllers do not support the extended Modbus functionality of other ranges of SCADAPack controllers.)

Simple Modbus Modbus If both Modbus drivers provide the required functionality, consider using the Advanced Modbus driver rather than the Simple Modbus driver. This will give you more flexibility should your system requirements change in the future.
SCADAPack x70

Monitoring and control

Device configuration management -Upload, import, export, download.

Firmware download

Download of security configuration

SCADAPack x70 DNP3 (using an application-specific extension)

Run the DNP3 driver along with the SCADAPack x70 extension driver.

This provides more feature-specific extended functionality for SCADAPack x70 devices than the Modbus, generic DNP3, or IEC 60870-5 drivers.

Monitoring and control

Advanced Modbus Modbus

Use the 'standard' and 'Generic' Modbus database items.

(SCADAPack x70 devices do not support the extended Modbus functionality of other ranges of SCADAPack controllers.)

Simple Modbus Modbus If both Modbus drivers provide the required functionality, consider using the Advanced Modbus driver rather than the Simple Modbus driver. This will give you more flexibility should your system requirements change in the future.
DNP3 DNP3

Use the 'standard' and 'Generic' DNP3 database items.

The SCADAPack x70 driver is only required if you intend to use Geo SCADA Expert to manage the configuration of the devices.

IEC 60870-5 IEC 60870-5-104 Use the IEC 60870-5 database items.
SCADAPack x70 (Realflo enabled)

Monitoring and processing of flow measurement data

Configuration of flow runs

Read flow run configuration

Write flow run configuration

SCADAPack Modbus Realflo Modbus (using an application-specific extension) Run the Advanced Modbus driver along with the SCADAPack Modbus and SCADAPack Modbus Realflo extension drivers.

Configuration of the SCADAPack x70 devices (to set up the mapping of the Modbus registers to the I/O)

Optionally monitor and control the non-Realflo device functionality (if you want a hybrid between DNP3 and Modbus data retrieval)

SCADAPack x70 DNP3 (using an application-specific extension)

Run the DNP3 driver along with the SCADAPack x70 extension driver.

(To read and configure the flow runs, you need to use the Modbus protocol, using the SCADAPack Modbus Realflo driver.)

Other SCADAPack ranges not mentioned separately in this table Monitoring and control DNP3 DNP3

Use the 'standard' and 'Generic' DNP3 database items.

(Other SCADAPack ranges do not support the extended DNP3 functionality of 386 eNET, SCADAPack E controllers, and SCADAPack x70 devices.)

Monitoring and control SCADAPack Modbus Modbus (using an application-specific extension) Run the Advanced Modbus driver along with the SCADAPack Modbus extension driver.
Realflo enabled SCADAPack controllers

Monitoring and processing of flow measurement data

Configuration of flow runs

Read flow run configuration

Write flow run configuration

SCADAPack Modbus Realflo Modbus (using an application-specific extension) Run the Advanced Modbus driver along with the SCADAPack Modbus and SCADAPack Modbus Realflo extension drivers.

586 eNET outstations are now known as SCADAPack ES outstations and Magna eNET outstations are now known as SCADAPack ER outstations. Both types of outstation are models in the SCADAPack E range of outstations.

For further information about any of the above drivers, see the relevant driver-specific guide. For example, for information about Realflo, see the Geo SCADA Expert Guide to the SCADAPack Modbus Realflo Driver. With those drivers that are extensions of other drivers, the driver guide for the extension driver will reference the guide for the 'parent' driver, as required.

Further Information

Supported Drivers and Protocols.


Disclaimer

Geo SCADA Expert 2022