Compressibility Approximated Flag
Associated with: Flow runs
This attribute displays the compressibility flag that presently applies to the Flow Run. The attribute is displayed once the server has retrieved Flow Run data from a Realflo-enabled SCADAPack controller.
Possible States:
- Compressibility value is calculated result
(Displayed when the flag is not set (reads 0)) - Compressibility value is approximate
(Displayed when the flag is set (reads 1)).